FB#.LINEPITCH

Description

This parameter defines the line pitch for linear encoders in nm per line. This is only used when using linear motor types. For rotary motors, see FB.ENCLINES.

Context

See Feedback # View and FB#.MECHTYPE.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

nm/line

Range

0.001 to 2000000.000

Default Value

20,000
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
FB1.LINEPITCH

3500h

0ah

Unsigned32

-

1000:1

Read/Write

No

FB2.LINEPITCH

3501h

0ah

Unsigned32

-

1000:1

Read/Write

No

FB3.LINEPITCH

3502h

0ah

Unsigned32

-

1000:1

Read/Write

No

FB4.LINEPITCH

3503h

0ah

Unsigned32

-

1000:1

Read/Write

No

FB5.LINEPITCH

3504h

0ah

Unsigned32

-

1000:1

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

FB1.LINEPITCH

30380

76AC

Unsigned32

Read/Write

-

FB2.LINEPITCH

30381

76AD

Unsigned32

Read/Write

-

FB3.LINEPITCH

30382

76AE

Unsigned32

Read/Write

-

FB4.LINEPITCH

30383

76AF

Unsigned32

Read/Write

-

FB5.LINEPITCH

30384

76B0

Unsigned32

Read/Write

-

PROFINET

Parameter

PNU

Data Type

Access

Units

FB1.LINEPITCH

30380

Float

Read/Write

-

FB2.LINEPITCH

30381

Float

Read/Write

-

FB3.LINEPITCH

30382

Float

Read/Write

-

FB4.LINEPITCH

30383

Float

Read/Write

-

FB5.LINEPITCH

30384

Float

Read/Write

-